Delete a program

A program contains routines, including a main routine and tags.
Delete programs from the
System
explorer. Deleting a parent program deletes the programs the program contains.
  1. On the explorer bar, select System Icon
    System.
  2. Right-click a program and select
    Delete
    . The message
    Are you sure you want to delete this program
    appears.
  3. Select
    Delete
    . The program no longer appears in
    System
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal