Monitor ethernet node capacity

In
Properties
, use the information in
Ethernet Nodes Capacity
to monitor controller ethernet node usage.
  1. On the explorer bar, select Devices icon
    Devices
    .
  2. In
    Devices
    , select the controller.
  3. If
    Properties
    is not open, on the pane bar, select Properties icon
    Properties
    .
  4. In
    Properties
    , under
    Ethernet Nodes Capacity
    , monitor the controller memory usage. The
    Ethernet Nodes Capacity
    pane indicates the available nodes, used nodes, and total capacity.
    If the size of the project approaches or exceeds the total ethernet nodes capacity available in the controller, a message warns you about the limited or exceeded capacity. When the ethernet nodes capacity is exceeded, you cannot deploy to any controller types except ControlLogix 1756-L85 controllers.
    TIP: In the Execution explorer, click on the controller to view the Properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal