Export Stratix device configuration

Export a
Stratix
device configuration to back up a device configuration to a computer. The configuration contains either one or two configuration files.
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. In
    Devices
    , right-click a
    Stratix
    device, and then select
    Properties
    .
  3. In
    Properties
    , select
    Save/Restore
    , then select
    Export
    .
  4. In
    Export Device Configuration
    , complete the following steps:
    1. In the
      Config file
      view, select
      Export
      . The file exports to your configured browser download location.
    2. (optional) If the device also requires a Vlan file, select
      Next
      , then in the
      Vlan file
      view, select
      Export
      . The file exports to your configured browser download location.
    3. Select
      Next
      , then select
      Close
      .
  5. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal