Delete a controller

Delete a controller to remove the controller from the project. The tasks, programs, and allocations to Smart Objects for the controller are removed with the controller. Devices attached to a backplane or bus of the controller are moved to the
Unassigned
folder. Delete a controller from the
Devices
explorer.
To delete a controller
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. In
    Devices
    explorer, right-click the controller and select Delete
    Delete
    .
The controller is removed.
TIP: You have the option to delete a controller from the
Device list
by selecting
Device list
under the Devices explorer, right-clicking a controller in the
Device list
tab, and selecting Delete
Delete
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal