Add a ladder diagram rung to a routine

Add a rung to a routine so that you can add branches and instructions to the rung.
Prerequisites
To add a ladder diagram rung to a routine
  1. In the Ladder Editor
    Toolbox
    , drag a rung Rung Icon to the canvas of the routine. Valid drop zones are indicated by Valid Drop Location Indicator.
    TIP: If
    Toolbox
    is not visible, on the pane
    bar, select Toolbox Icon
    Toolbox
    .
  2. TIP: Open the code editor to edit a ladder diagram rung in the Code Editor. For assistance, see Ladder routine structure and Ladder routine example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal