Add a ladder diagram branch level

Add a branch level to add an additional level to an existing ladder diagram branch. Instructions that you place in a branch level instruct the routine to use either the instruction in the branch level or the instruction in another branch level.
Prerequisites
To add a ladder diagram branch level
  1. In the ladder diagram, select a branch.
  2. From the Ladder Editor
    Toolbox
    , drag
    Branch Level
    Branch Level Icon to a valid drop zone in the rung. Valid drop zones are indicated by Valid Drop Location Indicator.
    TIP: If
    Toolbox
    is not open, in the pane bar, select Toolbox Icon
    Toolbox
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal