Launch the Unit Profile from the IntelliCENTER explorer

Use the
Unit Profile
tab to view detailed unit information in the IntelliCENTER lineup. View the:
  • device name
  • device type
  • IP address
  • MCC Network number
  • vendor code
  • product type
  • product code
  • major revision
  • minor revision
To launch the Unit Profile from the IntelliCENTER explorer
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. Select the
    IntelliCENTER
    tab.
  3. In the
    IntelliCENTER
    explorer, right-click a unit within a lineup and select
    Unit Profile
    to launch the Unit Profile and to view the unit information.
  4. (optional) To view unit documentation, under
    Documentation
    , select the
    Drawings
    ,
    Manuals
    , or
    Spares
    link.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal