Allocate FactoryTalk Smart Object or program to a controller and task

Allocate an existing
FactoryTalk Smart Object
or program to a controller or task.
  1. In the explorer bar, select System Icon
    System
    .
  2. Select the
    FactoryTalk Smart Object
    or program.
    TIP:
    Properties > Size
    shows how large the Smart Object or program is.
    Size
    is stated in blocks of memory and is the sum of all the programs belonging to the Smart Object.
  3. In
    Properties
    , select the
    Allocation
    tab and select:
    • Controller
      . Select a controller from the list to allocate the program of
      FactoryTalk Smart Object
      to a controller.
      • Select
        None
        to leave the program or
        FactoryTalk Smart Object
        unassigned.
    • Task
      . Select a task from the list to allocate the controller to a task.
      • Select
        None
        to leave the controller unassigned
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal