Online and offline indicators in the Explorer pane

You can edit a project or project components while online with a controller. The edits you make are offline-only until you redeploy the project.
This table lists indicators and examples of components that are online, offline, or both.
TIP: The green rail in the Explorer pane indicates that an element is included in the online workspace. It does not indicate that logic is executing.
Status
Indicator
Example
Elements are in the offline workspace.
Elements are in the online workspace.
Child components have an online or offline-only state that is different from the parent, so a dashed circle appears around the parent icon.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal