Select a FactoryTalk Vault solution

Select a FactoryTalk Vault solution to store your converted controller project files when you create a project.
TIP: If there is an error connecting to the Vault when creating a project, you will receive a notification to select a FactoryTalk Vault solution when pushing changes to the remote repository.
FactoryTalk Vault is a centralized solution to securely store documents, manage data access, and collaborate on projects.
  1. Select one of these options for a FactoryTalk Vault solution:
    • Select an exiting solution
    • Create solution
  2. Select
    Create
    to place your project in the FactoryTalk Vault solution.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal