Delete a project

Delete a project from the
Open project
dialog.
  1. Close any open project.
  2. Either:
    • On the
      Welcome
      page, select
      Open project
      .
    • From the menu bar, select
      File > Open project
      .
  3. In
    Open project
    dialog, in the
    Project Name
    list, hover over the project that you want to delete.
  4. Select the trash bin icon on the right to delete the project.
The project is only deleted from your workspace. The remote project and other user's copy of the project in their workspace will still exists.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal