Copy a project to a different organization
This feature allows you to copy a project to another organization to which you have
access.
NOTE:
To send a copy of a project, you must have be a member of
both the source and the target organizations. You must have an
Engineer
role
in the source organization. You can have any role in the target organization. Both
source and target organizations must have an active entitlement. You must also have
access to FactoryTalk Design Studio in the target organization where you want to
send the project copy.To copy a project to a different organization:
- Open the project you want to copy.
- In File selectSend a copy. TheSend copy to another organizationdialog appears.
- In theOrganization Namedrop-down list select the organization to which you want to send the copy. Only organizations with an active FactoryTalk Design Studio entitlement can be selected.
- Enter a name for the copy in theNamesection.
- Check theKeep project historycheckbox if you want to keep a list of the history of the copies.
- SelectCopy. A status bar indicates the copy progress, which can take several minutes to complete.
An email is sent to the all administrators of the source
tenant, letting them know that a project has been copied out of their organization.
Another email goes to the user who initiated the project transfer, letting them know
that the copy to another organization was successful. If a copy fails, an email
only
goes to the user who initiated the copy to let them know the copy was
unsuccessful.Provide Feedback