Delete a duplicate routine implementation
When you create a routine, it contains the forward declaration and the implementation. If
the implementation is copied and creates a duplicate implementation, you receive the
error
RoutineName Routine implementation already exists. To avoid unexpected
results, create a unique routine name. Error code: DS0177.
You must
delete the duplicate implementation file to resolve this error.To delete a duplicate routine implementation
- Open the Code Editor from the routine element by right clicking the element and selectingCode Editor.
- In the Code Editor, navigate to the line number and Character column of the error message, then select the routine implementation that you want to delete.
- Select
to the left of the component to open the Code Actions menu.
- SelectDelete duplicate implementation.
Provide Feedback