Delete a duplicate program implementation
When you create a program, it contains the forward declaration and the implementation. If
the implementation is copied and creates a duplicate implementation, you receive the
error
ProgramName Program implementation already exists. To avoid unexpected
results, create a unique program name. Error code: DS0182.
You must
delete the duplicate implementation file to resolve this error.To delete a duplicate program implementation
- Open the Code Editor from the program element by right clicking the element and selectingCode Editor.
- In the Code Editor, navigate to the line number and Character column of the error message, then select the program implementation that you want to delete.
- Select
to the left of the component to open the Code Actions menu.
- SelectDelete duplicate implementation.
Provide Feedback