Create a missing program implementation
When you create a program, it contains the forward declaration and the implementation.
The forward declaration contains the
extern
keyword, such as
extern program myProgram()[];
. If the forward declaration is specified but the implementation does not exist, you
receive the error
Missing implementation for external program ProgramName.
Add a valid implementation. Error code: DS0171.
You must create the
missing program implementation file to resolve this error.To create a missing program implementation
- Open the Code Editor from the program element by right clicking the element and selectingCode Editor.
- In the Code Editor, navigate to the line number and Character column where you want to create the missing program implementation.
- Select
to the left of the component with the missing implementation to open the Code Actions menu.
- SelectCreate missing program implementation.
Provide Feedback