Data Context

Use
Data Context
to view all invocations of an Add-On Instruction (AOI) across a project. Data Context provides a list of where each AOI is used, including its fully qualified name and the structure of any AOIs containing it, if it is nested within other AOIs.
IMPORTANT: If
Data Context
is opened from an online routine, it will only show information about AOI invocations within the online controller. AOIs elsewhere in the project are not shown. To view the data context for offline AOI invocations, open
Data Context
from the
Library
pane.
To open
Data Context
:
  1. In the program ladder diagram, right-click the Add-On Instruction invocation, then select either
    Open instruction parameters
    or
    Open instruction logic
    .
  2. In the
    Add-On Instruction Instance Tab
    or
    Add-On Instruction Routine Editor
    , select the drop-down list in the upper right that shows the name of the AOI invocation.
Data context fields and properties
Field or Property
Description
Search
Enter text in the search field to filter the list of AOI invocations by the search term. Results may match any value in any invocation within the list. Results are highlighted in bold.
Name
The name of the backing tag used in the AOI invocation.
Tag Scope
The name of the AOI invocation starting from the project to the selected AOI invocation.
Controller Application
The name of the controller application to which this AOI invocation is assigned.
Innermost Parent
If the AOI invocation is nested within one or more AOI invocations, this displays the AOI invocation one nested level up from the selected invocation.
Outermost Parent
If the AOI invocation is nested within one or more AOI invocations, this displays the AOI invocation from the selected invocation.
Path
The names of the programs, routines, rungs, and objects that contain the outermost AOI invocation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal