Tangent (TAN)

The TAN instruction takes the tangent of the Source value (in radians) and stores the result in the Destination.
The TAN operator or function computes the tangent of Source and returns the floating point result.
Available Languages
Ladder Diagram
Ladder Diagram_Tangent (TAN)_v1
FactoryTalk Design Studio
DSL - Ladder Diagram
Operands
IMPORTANT: Unexpected operation may occur if:
  • Output tag operands are overwritten
  • Members of a structure operand are overwritten
  • Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Ladder Diagram
Operand
Data Type
Format
Description
Source
SINT
INT
DINT
LINT
USINT
UINT
UDINT
ULINT
REAL
LREAL
Immediate
tag
Value to convert to tangent.
Destination
SINT
INT
DINT
LINT
USINT
UINT
UDINT
ULINT
REAL
LREAL
tag
Tag to store result of the instruction.
Operator Aspects
The TAN operator can be used in various expressions. Both applications of TAN return a floating point result containing the tangent of the Source. Depending on the context, this value may then be type converted if appropriate.
Affects Math Status Flags
Conditional, see Math status flags
.
Major/Minor Faults
None specific to this instruction. See Index through arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
N/A
Rung-condition-in is false
Set Rung-condition-out to Rung-condition-in.
Rung-condition-in is true
Set Rung-condition-out to Rung-condition-in.
Dest = tangent value of the Source.
Postscan
N/A
Example
Ladder Diagram
FTStudio-TAN-LD-EX-V1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal