Controlling a Ratio (PID)

u can maintain two values in a ratio by using these parameters:
  • Uncontrolled value
  • Controlled value (the resultant setpoint to be used by the PID instruction)
  • Ratio between these two values
Relay Ladder
FTStudio-PID-LD-EX2-V1
TIP:
Tip: To avoid locking up the PID with invalid internal floating point values, ensure the PV is not INF or NAN before invoking the instruction such as:
XIC (PC_timer.DN)
MOV(Local:0:1.Ch0Data, Local:0:1.Ch0Data)
XIO(S:V)
PID(...)
For this multiplication
Enter this value
Destination
Controlled value
Source A
Uncontrolled value
Source B
Ratio
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal