Masked Move (MVM)

The MVM instruction copies the Source to a Destination and allows portions of the data to be masked.
The MVM instruction uses a Mask to pass or block Source data bits. A "1" in the mask means the data bit is passed; a "0" in the mask means the data bit is blocked.
If integer data types are mixed, the instruction fills the upper bits of the smaller integer data types with 0s so that they are the same size as the largest data type.
Entering an immediate mask value
When mask is entered, the programming software defaults to decimal values. To enter a mask using another format, precede the value with the correct prefix.
Prefix
Description
16#
Hexadecimal (e.g., 16#0F0F)
8#
Octal (e.g., 8#16)
2#
Binary (e.g., 2#00110011)
Available Languages
Ladder Diagram
Ladder Diagram_Masked Move (MVM)_v1
FactoryTalk Design Studio
DSL - Ladder Diagram
Operands
There are data conversion rules for mixed data types within an instruction. See Data conversions.
Ladder Diagram
Operand
Data Type
Format
Description
Source
SINT
INT
DINT
immediate
tag
Value to move
Mask
SINT
INT
DINT
immediate
tag
Which bits to block or pass
Dest
SINT
INT
DINT
tag
Tag to store the result
Affects Math Status Flags
No
Major/Minor Faults
A minor fault will occur if:
Fault Type
Fault Code
The feature is enabled and overflow is detected
4
4
See Index through arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
N/A
Rung-condition-in is false
N/A
Rung-condition-in is true
The instruction passes the Source through the Mask and copies the result into the Destination. Unmasked bits in the Destination remain unchanged.
Postscan
N/A
Example
Ladder Diagram
L5K_MVM Ladder Diagram Example
Row 1: value_b before MVM
Row 2: value_a
Row 3: mask_2
Row 4: value_b after MVM
FTStudio-MVM-LD-EX-V1
Copy data from value_a to value_b, while allowing data to be masked (a 0 masks the data in value_a).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal