Mask Equal To (MEQ)

The MEQ instruction passes the Source and Compare values through a Mask and compares the results.
Available Languages
Ladder Diagram
Ladder Diagram_Mask Equal To (MEQ)_v1
Operands
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Ladder Diagram
Operand
Data Type
Format
Description
Source
SINT
INT
DINT
LINT
USINT
UINT
UDINT
ULINT
immediate
tag
Value to test against Compare.
Mask
SINT
INT
DINT
LINT
USINT
UINT
UDINT
ULINT
immediate
tag
Which bits to block or pass.
Compare
SINT
INT
DINT
LINT
USINT
UINT
UDINT
ULINT
immediate
tag
Value to test against Source.
Operation
A "1" in the mask means the data bit is passed. A "0" in the mask means the data bit is blocked. Typically, the Source, Mask, and Compare values are all the same data type.
If using SINT or INT data type, the instruction fills the upper bits of that value with 0s so that it is the same size as the DINT data type.
Enter an immediate mask value
When entering a mask, the programming software defaults to decimal values. To enter a mask using another format, precede the value with the correct prefix.
Prefix
Description
16#
hexadecimal, such as 16#0F0F
8#
octal, such as 8#16
2#
binary, such as 2#00110011
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index through arraysfor array-indexing faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
N/A
Rung-condition-in is false
Set Rung-condition-out to Rung-condition-in.
Rung-condition-in is true
Refer to MEQ Flow Chart (True).
If output is true
Set Rung-condition-out to true
else
Clear Rung-condition-out to false
Postscan
N/A
MEQ Flow Chart (True)
MEQ_Flow Chart True
Examples
Example 1
If the masked value_1 is equal to the masked value_2, set light_1 to true. If the masked value_1 is not equal to the masked value_2, clear light_1 to false.
This example shows that the masked values are equal. A 0 in the mask restrains the instruction from comparing that bit (indicated by an x in the example).
Ladder Diagram
MEQ Example 1
FTStudio-MEQ-LD-EX1-V1
Example 2
If the masked value_1 is equal to the masked value_2, set light_1 to true. If the masked value_1 is not equal to the masked value_2, clear light_1 to false.
This example shows that the masked values are not equal. A 0 in the mask restrains the instruction from comparing that bit (indicated by an x in the example).
Ladder Diagram
MEQ Example 2
FTStudio-MEQ-LD-EX2-V1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal