Insert String (INSERT)

Use the INSERT instruction to add ASCII characters to a specified location within a string.
The INSERT instruction adds the characters in Source B to a designated position within Source A and places the result in the Destination.
  • Start defines where in Source A that Source B is added.
Unless Source A and the Destination are the same tag, Source A remains unchanged.
Available Languages
Ladder Diagram
Ladder Diagram_Insert String (INSERT)_v1
FactoryTalk Design Studio
DSL - Ladder Diagram
INSERT (SourceA,SourceB,Start,Dest);
Operands
There are data conversion rules for mixed data types within an instruction. See Data Conversion. The INSERT instruction uses the following operands.
Ladder Diagram
Operand
Type
Format
Description
Notes
Source A
String type
Tag
String to add the characters to
String types are default STRING data types or any new string types you create
Source B
String type
Tag
String containing the characters to add
Start
SINT
DINT
Immediate tag
Position in Source A to add the characters
Enter a number between 1 and the DATA size of the Source.
Destination
String type
Tag
String to store the result
Affects Math Status Flags
No
Major/Minor Faults
Type
Code
Cause
Recovery Method
4
51
The LEN value of the string tag is greater than the DATA size of the string tag.
  1. Check that no instruction is writing to the LEN member of the string type tag.
  2. In the LEN value, enter the number of characters that the string contains.
4
56
The Start or Quantity value is invalid.
Check that the Start value is between 1 and the DATA size of the Source.
Execution
Ladder Diagram
Condition
Ladder Diagram Action
Prescan
The rung-condition-out is set to false.
Rung-condition-in is false
The rung-condition-out is set to false.
Rung-condition-in is true
The instruction executes.
The rung-condition-out is set to true.
Postscan
The rung-condition-out is set to false.
Example
When
temp_high
is set, the INSERT instruction adds the characters in
string_2
to position 2 within
string_1
and places the result in
string_3
.
Ladder Diagram
FTStudio-INSERT-LD-EX-V1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal