Upper Case (UPPER)

The UPPER instruction converts the alphabetical characters in a string to upper case characters.
The UPPER instruction converts all the letters in the Source to upper case, and places the result in the Destination.
  • ASCII characters are case-sensitive. Upper case A ($41) is not equal to lower case a ($61).
  • If operators directly enter ASCII characters, convert the characters to all upper case or lower case before you compare them.
Any characters in the Source string that are not letters remain unchanged.
Available Languages
Ladder Diagram
Ladder Diagram_Upper Case (UPPER)_v1
FactoryTalk Design Studio
DSL - Ladder Diagram
UPPER(Source,Dest);
Operands
Ladder Diagram
Operand
Type
Format
Description
Source
String
tag
Tag that contains the characters you want to convert to upper case
Destination
String
tag
Tag to store the characters in upper case
Affects Math Status Flags
No
Major/Minor Faults
Type
Code
Cause
Recovery Method
4
51
The LEN value of the string tag is greater than the DATA size of the string tag.
Check that no instruction is writing to the LEN member of the string type tag.
In the LEN value, enter the number of characters that the string contains.
4
52
The output string is larger than the destination
Create a new string type that is large enough for the output string. Use the new string type as the data type for the destination.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
N/A
Rung-condition-in is false
N/A
Rung-condition-in is true
The instruction executes.
Postscan
N/A
Example
To find information about a specific item, an operator enters the catalog number of the item into an ASCII terminal. After the controller reads the input from a terminal (terminal_read is set), the UPPER instruction converts the characters in catalog_number to all upper case characters and stores the result in catalog_number_upper_case. A subsequent rung then searches an array for characters that match those in catalog_number_upper_case.
Ladder Diagram
FTStudio UPPER LD EX V1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal