REAL to String (RTOS)

The RTOS instruction produces the ASCII representation of a REAL value.
The RTOS instruction converts the Source to a string of ASCII characters and places the result in the Destination.
Available Languages
Ladder Diagram
Ladder Diagram_REAL to String (RTOS)_v1
FactoryTalk Design Studio
DSL - Ladder Diagram
RTOS(Source,Dest);
Operands
Ladder Diagram
Operand
Type
Format
Description
Notes
Source
REAL
Tag
The tag that contains the REAL value
Destination
String type
Tag
The tag to store the ASCII value
String types are:
  • Default STRING data type
  • Any new string type you create
Affects Math Status Flags
No
Major/Minor Faults
Type
Code
Cause
Recovery Method
4
52
The output string is larger than the destination
Create a new string type that is large enough for the output string. Use the new string type as the data type for the destination.
See Index through arrays for operand-related faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
N/A
Rung-condition-in is false
N/A
Rung-condition-in is true
The instruction executes.
Postscan
N/A
Examples
When send_data is set, the RTOS instruction converts the value in data_1 to a string of ASCII characters and places the result in data_1_ascii. Subsequent rungs insert or concatenate data_1_ascii with other strings to produce a complete message for a display terminal.
Ladder Diagram
FTStudio RTOS LD EX V1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal