Array concepts

Arrays let you refer to a group of data (of the same data type) by the same name and to use a number (index) to identify an individual element. An element in an array can be a/an:
  • Atomic data type
  • Structure data type
You specify an element in an array by its subscript(s). Enter the array tag name followed by the subscript(s) in square brackets. The subscript(s) must specify a value for each dimension of the array. Dimensions are zero-based.
For this array
Specify
one dimension
array_name[subscript_0]
two one dimension
array_name[subscript_0, subscript_1]
three dimension
array_name[subscript_0, subscript_1, subscript_2]
An array can have as many as three dimensions. The total number of elements in an array is the product of each dimension’s size.
This array:
Stores this data:
Example:
one dimension
one-dimension array
Tag name
Type
Dimension 0
Dimension1
Dimension 2
one_d_array
DINT[7]
7
--
--
total number of elements = 7
valid subscript range DINT[x] where x=0-6
two dimension
two-dimension array
Tag name
Type
Dimension 1
Dimension 0
Dimension
two_d_arry
DINT[4,5]
4
5
--
total number of elements = 4 * 5 = 20
valid subscript range DINT[x,y] where x=0–3; y=0–4
three dimension
multi-dimension array
Tag name
Type
Dimension 2
Dimension 1
Dimension 0
three_d_array
DINT[2,3,4]
2
3
4
total number of elements = 2 * 3 * 4 = 24
valid subscript range DINT[x,y,z] where x=0–1; y=0–2, z=0–3
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal