Entitlements and timed trials

Entitlements and timed trials provide access to different functionality at no cost, for a fee, or for a trial period.
Access to
FactoryTalk Design Studio®
is granted by allocating entitlements to FactoryTalk Hub organizations. Entitlements determine the level of functionality available to the user within
FactoryTalk Design Studio
. For more information on using entitlements in FactoryTalk Hub, see View Entitlements.
FactoryTalk Design Studio
entitlements are specific to a single FactoryTalk Hub organization and are available to any user with
FactoryTalk Design Studio
access on a first-come, first-served basis. Users claim an entitlement upon logging into
FactoryTalk Design Studio
and consume that user seat for the duration of their activity. Entitlements and their corresponding user seats are available in two tiers: Basic and Core.
Entitlement seats are released when a user is no longer active in
FactoryTalk Design Studio
. The entitlement will remain assigned to the user for 15 minutes after they leave their session, or the user can select the
Log Out
option to immediately return the entitlement seat back to the pool within the FactoryTalk Hub organization.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal