Design considerations

When designing your application, consider:
  • Element scope
    . The boundary where an element and its content can be accessed. Every element in
    FactoryTalk Design Studio
    defines a scope.
  • Element references
    . When one element refers to another element. References must be valid. For example:
    • An instruction references a tag as an argument to a parameter.
    • A tag references a data type to declare the type of the tag.
    • A tag references a program to be scheduled within that task.
  • Format of element references
    . There are multiple formats that can reference an element:
    • Fully qualified name that explicitly names the referenced element
    • Partially qualified name that identifies matching qualified names in the referenced element
    • Element name
    • Owner scope operators
  • Role-Based Access Control
    . Access to capabilities in FactoryTalk Design Studio is based on the user's role. The three roles are:
    • Guest
    • Engineer
    • Administrator
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal