Toolbar

Icons in the toolbar include:
Icon
Description
Device list icon
Device list
. Opens the
Device list
to view and set controller and device properties.
Commit icon
Commit
. Save changes to the local repository.
Push icon
Push
. Transfer commits from the local repository for the shared project to the remote repository. The number in the icon identifies the total commits made by the current user (local commits).
Pull icon
Pull
. Update the local repository of the shared project from the remote repository. The number in the icon identifies the total commits made by other users sharing the project (remote commits).
The
Change history
tab shows all changes committed to the repository for a local or shared project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal