Pane bar

Use the Pane Bar icons to toggle the visibility of panes at specific locations in the user interface.
Item
Description
Left Pane icon
Left panes
. Toggle the panes on the left side of the user interface.
Explorer icon
Explorer
. Toggle the selected Explorer pane.
Right Pane icon
Right panes
. Toggle the panes on the right side of the user interface.
Toolbox icon
Toolbox
. Toggle the
Toolbox
of instructions to add to a ladder diagram and an Add-On Instruction.
Properties icon
Properties
. Toggle the
Properties
pane for the selected element.
Bottom Pane icon
Bottom panes
. Toggle the panes at the bottom of the user interface.
Console icon
Output
. Toggle the error, warning, and information messages that appear for the routines and instructions in the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal