bus object

Defines the logical topology of a set of connected devices, including the buses that connect devices.
bus [busType] [name] { <property name> := <property value>; ... <device>.<port> ... }
Property
Description
busType (required)
Type of bus.
name (required)
Name of the bus. The name is auto generated: <busType name> +<sequential number>
busSize
Configured size of the bus. This property defines how many child devices can be connected at once. The min and max bus size is defined in the busType. Validations are included to give warnings or errors when this value is out of range.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal