Device structure in a project

This sample code shows device structure as it appears in a project.
projectRoot │ ├───devices │ │ output2.device │ │ adapter1.device │ │ input2.device │ │ controller2.device │ │ controller1.device │ │ adapter5.device │ │ input1.device │ │ │ └───types │ AB__1756_DI__C__1.device │ AB__1756_DO__O__0.device │ AB__1756_DI__I__0.device │ AB__1756_ENET_SLOT__O__0.device │ AB__1756_DO__I__0.device │ AB__1756_ENET_SLOT__I__0.device │ AB__1756_ENET_7SLOT__O__0.device │ AB__1756_OF8_Float__C__0.device │ AB__1756_OF8_Float__I__0.device │ AB__1756_OF8_Float__O__0.device │ AB__1756_NIO_Struct__C__0.device │ AB__1756_ENET_7SLOT__I__0.device │ AB__1756_DO__C__0.device └───topologies topology.device
Devices
Each device is stored as a
.device
file. All
.device
files are checked into the version control system (VCS).
Module-defined types
Types are defined by the Device Catalog and are created when the device is created. Comments in the file and in the help content instruct users not to manually modify this data.
Topologies
Each topology is represented by its own
.device
file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal