Standard toolbar

The standard toolbar provides you with many standard functions that you will use frequently as you develop your logic program.
standard_toolbar_v31
These functions are:
  • New project, Open project, Save project
  • Print
  • Cut, Copy, Paste
  • Undo, Redo
  • Find Next, Find Previous, Find All (either by typing what you wish to find in the search box on the toolbar and clicking on the Find buttons, or by clicking on those buttons and accessing the Find and Find Within dialog boxes)
  • Toggle Controller Organizer
  • Toggle Logical Organizer
  • Verify Routine, Verify Controller
  • Build (Creates binary files compiled from user subroutines and caches them in the project .ACD file. If these binary files are present in the project during a download, then Logix Designer does not have to recompile them, saving time during the download process.)
    TIP:
    Tooltips on the toolbar indicate the intended use of each tool. Simply move your cursor over the icon and the tooltip appears.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal