The attempted command cannot be executed with the axis in shutdown state

Certain commands, such as Tune and Motor/Encoder Test, cannot be executed if the servo is in SHUTDOWN state. Execute the shutdown reset command, and then retry the command.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal