Clearing faults in Run mode

If the controller keyswitch is in the RUN position, clearing the faults returns the controller to Run mode. This restarts the execution of the routines in the controller.
If the keyswitch is in the REM position, clearing the faults always returns the controller to Remote Program mode. Execution of the routines in the controller will not restart.
Select
Yes
if you want to proceed with clearing the faults, or
No
if you wish to cancel this operation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal