Remove the unit of measure from a variable
    Remove the unit of measure for a variable to no longer have the value for that variable appear in that unit of measure.
- InProject view, select a variable.
- InProperties, select the unit of measurement in the value of the variable.
- Select<None>and then chooseSelect.
The unit of measure is removed from the variable.
Provide Feedback