Source Control > Check Out command

Choose this command to initiate a check out operation.
Note that this menu item displays only if all of the following conditions exist:
  • an open project exists
  • either the
    Logix Designer
    application has automatically drawn an association between the open project and one under source control, or you have explicitly established that association.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal