Module Properties - SERCOS Interface

Use the SERCOS Interface tab for the:
  • 1756-M03SE
  • 1756-M08SE
  • 1756-M16SE
  • 1768-M04SE
  • 1784-PM16SE
  • Embedded SERCOS Interface
Use this tab to set and display the:
  • SERCOS baud rate,
  • update rate for the SERCOS ring, and
  • fiber optic transmit power range for the SERCOS ring.
The SERCOS ring consists of the drives and axes connected to a motion module.
Parameters
Data Rate
Select the baud rate for the SERCOS ring. (For this release, this value is set to 4 MB and is Read Only.)
Cycle Time
Select the update rate for the SERCOS ring.
Transmit Power
Select the optic transmit power range for the SERCOS ring. Choose from High or Low.
Status
Displays the status the controller has about the module:
Status Name
Description
Standby
a transient state that occurs when shutting down
Faulted
unable to communicate with the module. When the status is Faulted, the Connection tab displays the fault.
Validating
a transient state that occurs before connecting to the module
Connecting
a state that occurs while the connection(s) are being established to the module
Running
the module is communicating and everything is working as expected
Shutting Down
the connections are closing
Inhibited
the connection to the module is inhibited
Waiting
a connection to this module has not yet been made due to one of the following:
  • its parent has not yet made a connection to it
  • its parent is inhibited
  • its parent is faulted
Offline
you are not online
OK
Click this button to accept your edits and close the dialog.
Cancel
Click this button to cancel your edits and close the dialog.
Apply
Click this button to apply your edits and continue editing.
Help
Click this button for help on this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal