Error reading the list of running drivers from RSLinxClassic or FactoryTalk Linx

This error occurs after shutting down
RSLinx Classic
or
FactoryTalk Linx
while the
Logix Designer
application is still running, and then selecting a driver in the application. Shut down and restart the application.
This error also occurs if
RSLinx Classic
or
FactoryTalk Linx
is not installed, or if there is a problem with the
RSLinx Classic
or
FactoryTalk Linx
installation on the computer.
For assistance with
RSLinx Classic
FactoryTalk Linx
or
FactoryTalk Linx
, contact Rockwell Automation Technical Support.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal