Error - Failed to logon to database

You failed to associate the current project with any project under source control because of one of the following reasons and source control operations will not be available for this project.
  • You entered an invalid username or password,
  • You entered an invalid server or database entry,
  • You lost connection to the server.
OK
Click this button to close the dialog box and open either a copy of the file or a standard, writable project with only the Add to Source Control menu item available.
Help
Click this button for help on this error.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal