View Program Performance Details

View specific details of your program/phase operations in the Monitor tab. From this tab, view information on maximum and last scan times. Scan time information is not available for folders.
Click the
Reset Max
button to reset these values and restart the timer.
TIP: To open the Program Properties dialog box:
  • From either the Controller Organizer or Logical Organizer, right-click the program to change and choose
    Properties
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal