Paste Special > Without Connections

Choose this command to paste a program without its parameter connections in the Controller Organizer or the Logical Organizer. You can also use Paste Special without Connections when pasting a folder in the Logical Organizer. This is useful when the copied parameter connections are not available in the destination project.
Paste Special > Without Connections is also available when copying from the Controller Organizer to the Logical Organizer, or vice versa.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal