Backlash page

The settings on the
Backlash
page configure backlash options for the load of the motor. Use the settings to:
  • Enter the
    Reversal Offset
    value to compensate for positional inaccuracy introduced by mechanical backlash.
  • Enter the
    Compensation Window
    value to define a window around the command position.
TIP: To open the Backlash page:
  1. In the
    Controller Organizer
    , expand the
    Motion Groups
    folder, and double-click an axis.
  2. From the
    Axis Properties
    dialog box, in
    Categories
    , expand the
    Load
    folder, and then click
    Backlash
    .
Parameter
Description
Reversal Offset
Specifies the reversal offset for the load in terms of user-defined position units.
Compensation Window
Specifies the compensation window in terms of user position units.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal